AXIS#.HOME.AUTOMOVE

Description

AXIS#.HOME.AUTOMOVE specifies whether the axis starts the configured homing move when the axis is enabled.


  • When Axis 2 is configured as a gantry (AXIS2.CMDSOURCE = 4), AXIS1.HOME.AUTOMOVE configures the automatic homing behavior for both Axis 1 and Axis 2. The drive ignores AXIS2.HOME.AUTOMOVE.
Value Description
0 The axis never starts a homing move when the axis is enabled.
1

The axis starts a homing move when the axis is enabled.

This homing move is skipped if:

The axis is already homed

The axis is not in position mode (AXIS#.OPMODE= 2)

The axis is not in service mode (AXIS#.CMDSOURCE= 0).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

AXIS#.HOME.MODE

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.HOME.AUTOMOVE

5008h

04h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6101

1

6101 (0x17d5)

AXIS1.HOME.AUTOMOVE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.HOME.AUTOMOVE

6101

Unsigned8

Read/Write

-

Related Topics

Homing